Other Parts Discussed in Thread: MSP430G2553, MSP430FR5739
Hi Guys,
I am working on SPI with a MSP430 as master and need to keep a slave device high to disable it (or at least that's what's recommended). It the MSP is off (i.e. LPM3 or 3.5 depending on which platform I'll be using) can the /SS output pin be kept high whilst the MSP is asleep (don't think so...)?
If not what's the best way around this? Should I just keep the line low anyway as no signal is fired from the MSP?
Thanks