Hi Team,
A customer has some questions on the MSP430F5438:
1. The MSP430 is configured as a SPI master. When doing a multi-byte transfer using DMA what is the maximum intra-byte delay time seen on spi bus pins?
(I’ve looked at the pins using an o’scope and I do not see a measurable delay.)
2. On page 56 of MSP430F5438:
1. What are the SPI timing values (tsu, thd, etc) when the voltage level is 3.3V (Datasheet only specifies 2.5 & 3V) ?
2. On that same page why is there an additional data bits seen on the SIMO lines (after the final SPI clk bit)?
3. On the same page is UCLK equivalent to UCxCLK for the spi peripheral?
Your help is much appreciated! Thanks.
Regards,
Oscar