Other Parts Discussed in Thread: MSP430F1232
I'm using the MSP4302274. The specsheet claims a minimum endurance of 10k cyles. I'm unsure how these are calculated. Is a cycle a write OR an erase, or a write AND an erase?
Each segment is made up of 32 16-bit words. If I were to write into each of those 32 words (sequentially), then erase the segment, and repeat the process 9 times (so 10 times total), how many cycles would I have burned up for each cell? 10 or 20?