Other Parts Discussed in Thread: MSP-EXP430F5529LP
Hello,
I am using a MSP-EXP430F5529LP and a MSP-EXP430G2 for I2C test. The F5529 as a master receive data from G2553 as a slave.The code is examples MSP430F55xx_uscib0_i2c_04 and msp430g2xx3_uscib0_i2c_05 from CCS
However,it does not work.And when a start condition is sent ,the UCNACKIFG of F5529 is set.What wrong did I do?
PS:I use two 10K Pull up resistors. Slave address is set as 0x48.Is it right? I have tested it as 0x24 and the result is the same.
Thanks for your help.