When will this errata be fixed?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Which MSP are you exactly talking about?
In the specific 6736 errata sheet is no trace of DMA9. (during the last years, the more common sub-family errata sheets have been replaced with individual errata sheets for single devices)
So maybe you have a version of a more generic errata sheet which is obsolete already and won't be updated anymore.
Sorry.
MSP430F67691 Device Errata sheet
SLAZ509H–January 2013–Revised May 2014
I see. This is 67xx1 sub-family. (and there’s even 67xx1A sub-family)
Yes, the erratum is there and has been discussed here in the forum for some time. Since you still can use USCIB for high-speed SPI with DMA, it isn’t as bad as it looks at first. (I’m using SPI and I2C on the same USCI simultaneously): For UART, you usually have enough time to handle the transfer with IRQ. But I agree that it is a nasty one and should be fixed.
Well, I can’t say when this will happen. And except a very few exceptions, TI will likely not release premature information about when something will be fixed or not. Like most other companies I know. The only big exception here is Microsoft: they announce things where development has not even started, just to bind customers and prevent them from buying from a competitor.
BTW: a suggested workaround was to use DMALEVEL to trigger a transfer as long as the interrupt is there (not edge triggered). Since the interrupt is cleared on the transfer, this might work. But I don’t remember what the outcome was. You may try and test :)
Well, then I don’t have an idea. Unfortunately, it affects RX as well as TX, or else you could (depending on SPI mode phase) the other one for a trigger (and do two DMA transfers) with proper priority order. But as it seems, there is really no workaround for UART and the only workaround for SPI is using USCIB.
**Attention** This is a public forum