Other Parts Discussed in Thread: MSP430F5529, MSP430F2418
I use "Proteus Tool 8.0 " to emulted my program. But in this tool does'nt have msp430f5529
So, can you show me how to add msp430f5529 into "Proteus tool"?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5529, MSP430F2418
Well, you’ll need to add the proper MSP design files to Proteus. I don’t know whether one is available from TI. If so, it is found on the MSP430F5529 product page. If not, you’ll have to look for them at the Proteus community – or create them yourself :) TI obviously can’t provide design files for all 3rd party programs someone might possibly use.
Hi Nanda,
I had simulated some MSP430 code over the proteus v7.10 and v7.8. Yeah some generally available and mostly Gxxxx series not available there in proteus.
So what you can do?? First compile the code for similar IC to f5529 available in proteus. And at last when you ready to use the code on hardware then just compile the same code for f5529. It realy works.
yeah but don't forget to set the proper clock of msp430 in simulation. If you have any problem regarding proteus then feel free to ask. If you start a topic regarding proteus then dont forget to mention the "proteus" keyword in title.
If further problem occurs then feel free to ask.
Good luck,
Regards,
Dharmendra Sharma
INDIA
__________________________________
Do, click "Verify Answer", if any of my replies helps solve your problem.
THX A LOT FOR YUR SUPPORT ..CAN YU PLEASE TELL ME THE RELATED TO f5529 IN PROTUS ...I DID WITH F249 MODEL ?? IS IT OKAY FOR NON INVASIVE GLUCOSE MONITORING
Hey Nanda,
First tell me which features of MSP are you using?? like GPIO, ADC, TIMER, UART etc.
Regards,
Dharmendra Sharma
INDIA
__________________________________
Do, click "Verify Answer", if any of my replies helps solve your problem.
Nanda,
You should us msp430f2418 for simulation. Since you are not using too much features so why you are using such a heavy MSP430?
Regards,
Dharmendra Sharma
INDIA
__________________________________
Do, click "Verify Answer", if any of my replies helps solve your problem.
**Attention** This is a public forum