Other Parts Discussed in Thread: MSP430F435
I have problem with Iar Embedded and MSP430 FET UIF with processore MSP430F435,
iI use this system and this processor from long time, without have problems.
from yesterday in the afternoon, when I try to program msp430f435 the system give me always the message that the itme is not supported. If I pick up a new item, start to program and when finisch give the message of error,
control the spy by wire or Jtag, and than exit from the emulation, later give always the message imet not supported.
is impossible later to program, also if I use Olimex system have the same error. If I use other bord with other processor with spy by wire, all work well. I try with 2 different computer , 3 different FET also FEt with LPM, and I try to remove the iar and install again, but not happens always the same, I think taht fire the internal fuse but I don't know why, all this board are already programmed and tested, If I go in the emulation without program ( with white icon) go inside withou any problem bu if I re- program have problem.
the firmware is ok because is already used from long time.
Luigi