Hi
After several tries I can’t program the EVM430F6779 Kit.
I’m using the IAR6.10 and the Olimex Tiny-V2.
I’m using an external power supply with 3.3 volts on the DGND and DVCC headers.
I don’t have the 230V connected to the board. I have The DVCC jumper in the “External” position, and all the J/S jumpers in the J position.
The result is always:
Communication Error
The log shows:
Mon Sep 01, 2014 11:46:49: Using license: Evaluation license - IAR Embedded Workbench for Texas Instruments MSP430, Evaluation Version 6.10
Mon Sep 01, 2014 11:46:50: Firmware version 20000007
Mon Sep 01, 2014 11:46:50: Interface dll version 2.0.0.7
Mon Sep 01, 2014 11:46:53: Unknown device : (InitEEM) , clientHandle=0x300b6f8
Can you please tell me what am I doing wrong?
Luis