Other Parts Discussed in Thread: MSP430F47126
I've been evaluating the SD16/SD16_A devices for using as an ADC and have a few questions:
* I've noticed that different documents have different information about whether the ADCs are separate or the inputs are multiplexed. I'm evaluating the MSP430F47126 for the moment. Does this have 6 separate sigma-delta cores or are the inputs multiplexed? Alternatively, is it possible to get ADC data from all 6 channels simultaneously at 32KHz, assuming I'm fine with 9-bit data.
* Can the individual ADCs, if they exist, be triggered simultaneously on this device? There were forum posts suggesting the bits were reserved.
* A signal range of 0.6V is fairly low for what I have in mind. At the moment I'm considering using Analog Devices' AD8475 on the signal to get +/- 1.2V range, though I'd like to be able to get a wider input range on the input. My signal sources are expected to be far away from the ADC and so far we've been using a +/- 5V differential pair to send the signals to the data acquisition system. Is there an appnote available or some pointers anyone could give me on how his sort of ADC input range can be effectively put to use?
* This question is probably overly subjective, but from the specs I've seen, I'm wondering if SD16 is better than ADC12 with oversampling. What are the use cases where SD16 becomes the better option?