Other Parts Discussed in Thread: MSP430F5438, MSP430F5438A, MSP430F5529
Hi,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5438, MSP430F5438A, MSP430F5529
Hi,
Jessica:
Here is one of the TI examples - it looks like you are close. (msp430x54xA_ta3_16.c)
//*******************************************************************************
// MSP430F543xA Demo - Timer_A3, PWM TA1.1-2, Up Mode, DCO SMCLK
//
// Description: This program generates two PWM outputs on P2.2,P2.3 using
// Timer1_A configured for up mode. The value in CCR0, 512-1, defines the PWM
// period and the values in CCR1 and CCR2 the PWM duty cycles. Using ~1.045MHz
// SMCLK as TACLK, the timer period is ~500us with a 75% duty cycle on P2.2
// and 25% on P2.3.
// ACLK = n/a, SMCLK = MCLK = TACLK = default DCO ~1.045MHz.
//
// MSP430F5438A
// -------------------
// /|\| |
// | | |
// --|RST |
// | |
// | P2.2/TA1.1|--> CCR1 - 75% PWM
// | P2.3/TA1.2|--> CCR2 - 25% PWM
//
// M. Morales
// Texas Instruments Inc.
// June 2009
// Built with CCE Version: 3.2.2 and IAR Embedded Workbench Version: 4.11B
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P2DIR |= 0x0C; // P2.2 and P2.3 output
P2SEL |= 0x0C; // P2.2 and P2.3 options select
TA1CCR0 = 512-1; // PWM Period
TA1CCTL1 = OUTMOD_7; // CCR1 reset/set
TA1CCR1 = 384; // CCR1 PWM duty cycle
TA1CCTL2 = OUTMOD_7; // CCR2 reset/set
TA1CCR2 = 128; // CCR2 PWM duty cycle
TA1CTL = TASSEL_2 + MC_1 + TACLR; // SMCLK, up mode, clear TAR
__bis_SR_register(LPM0_bits); // Enter LPM0
__no_operation(); // For debugger
}
Hi,
Thanks. I am trying just to get the output on one port pin P2.1 . I want the Timer A count from 327 to 654. Why my original code is not taking 327 into account? Why Timer A is not counting from 327 to 654? I expect my code to TURN the output high (P2.1) from 327 to 654 and then keep it low from 0 to 327.
jess
Hi Jessica,
There's a problem in using pin attached into the CCR0 like P2.1.
CCR0 is used to reset the timer. The timer simply counts up. When it reaches CCR0 it resets, and that set's the period.
CCR1 and CCR2 invert the output to 0 when their value is reaches and that way they control the duty to the pins they are attached too.
When the timer resets the output goes back to high, that happens when the CCR0 value is reached, if you are using the up mode.
I don't know if there is even a way to use CCR0 connected pins for PWM
you cant really use any pin connected to the CCR0 has a PWM output, only for other timer functions like capture
Luis, you can. However, using CCR0 for PWM requires additional software support. Let the timer run in cont mode then and change the CCRx values on each compare interrupt. This method can also be used if you need different cycle lengths for the CCRs (in up mode with plain hardware PWM, you have same cycle length for all CCRs, set by CCR0).
Jessica:
Is this a trick question from a professor?
It actually looks like you could get 50% (only) duty cycle by setting up the right mode and counting up and down, with a plus output on the up count and a ground on the down count. However, it is not adjustable at all, so it hardly qualifies as a "PWM." I think the solution I showed earlier from TI is a pretty good fit for what you really wanted.
**Attention** This is a public forum