At this time, VBUS to supply, but if it is not connected to Vcc, the problem occur?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi da,
I'm a bit confused to what your question is.
I'm guessing you have doubts about the MSP430F55xx launchpad power supply. You can use the USB 5V which will be regulated for the MCU.
You can also supply 5V or any acceptable voltage for the regulator (i can't remember from the top of my head th range) from another source into the VBUS. If you supply less than 5V into the VBUS it's a good idea do disconnect the programmer side by removing the jumper
You can also supply 3.3V, or any voltage in the MCU range to the VCC, but remember that is direct into the MCU so be careful
Thank you
Usually, it will be the power supply like this ...
Case 1
VBUS = 5v
VCC = 3.3v
Case 2
VBUS = 5v
VCC = VUSB (3.3v)
Case 3
VBUS = OFF
VCC = 3.3v
Do problem will occur when held in this state?
( MSP430 does not run in this state )
VBUS = 5v
VCC = OFF (0v)
Regards
I'm sorry, It is not a program.
The method of the supply of a power supply to MSP430F55x is as follows.
Case 1
VBUS(5v) power supply is connected to VBUS pin.
Vcc(3.3v) power supply is supplied to a DVCC pin.
Case 2
VBUS(5v) power supply is supplied to a VBUS pin.
VUSB pin is connected to a DVCC pin.
Case 3
VBUS power supply is connected to a ground.
Vcc(3.3v) power supply is connected to a DVCC pin.
Case X
VBUS power supply is connected to a VBUS pin.
DVcc pin is open.
When you connect only VBUS, is not connected to Vcc, and wanted to know MSP430F55xx whether from being destroyed.
> The MSP430 simply won't be powered.
May I take a MSP430 for the purpose of not breaking?
Regards.
The supply rails for the PHY (the physical USB layer) and the MSP are completely independent. One can be powered while the other isn’t. Usually, you use VBUS to source the included LDO voltage regulator to get the MSP supply voltage. So MSP is powered when VBUS is there. However, this is not a must. You can also use an ‘ideal ORing diode’ to power the MSP from VBUS if present and from a different supply, if not. (on some MSPs, you have a backup supply that can do this switch automatically)
I think da is trying to ask: Will the MSP be damaged or not if we connect VBUS pin of MSP to 5V power source while DVCC pins are unpowered.
Generally we should not apply power to any IO pin of the MCU when it is not supplied power. But it may be different this case of VBUS pin?
**Attention** This is a public forum