Other Parts Discussed in Thread: MSP430F2274
Hi, I'm working on the msp430f2274 and I need help regarding multiple analog channels. I'm using channels A0,A1,A2,A3,A4 and DTC to store the value in an array. But the values of each channel doesn't store in the array[#] correctly. For example in my code, value at A0 is suppose to be at samples[4], but it will appear on other samples[#] . There's a picture at the end to show what I meant. From the picture at the end. The top shows value(200+) of channel A0 on samples[4], then the next moment(bottom pic) shows value(200+) of channel A0 at samples[3].
#include <msp430.h>
#define BIT0 (0x0001)
#define BIT1 (0x0002)
#define BIT2 (0x0004)
#define BIT3 (0x0008)
#define BIT4 (0x0010)
#define BIT5 (0x0020)
#define BIT6 (0x0040)
#define BIT7 (0x0080)
#define BIT8 (0x0100)
#define BIT9 (0x0200)
#define BITA (0x0400)
#define BITB (0x0800)
#define BITC (0x1000)
#define BITD (0x2000)
#define BITE (0x4000)
#define BITF (0x8000)
// Global variables
unsigned int samples[5];
// Function prototypes
void ConfigureAdc(void);
void main(void)
{
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
BCSCTL1 = CALBC1_1MHZ; // Set range DCOCTL = CALDCO_1MHZ;
BCSCTL2 &= ~(DIVS_3); // SMCLK = DCO = 1MHz
P2SEL |= BIT4 + BIT3 + BIT2 + BIT1 + BIT0; // ADC input pin P2.4
P1REN = 0; // Pull-Up/Pull-down Resistors Disabled on P1 ports
P1SEL = 0; // Clear any previous settings
P1DIR = 0; // Clear any previous settings
P1OUT = 0; // Initialize port outputs to low state
P3REN = 0; // Pull-Up/Pull-down Resistors Disabled on P3 ports
P3SEL = 0; // Clear any previous settings
P3DIR = 0; // Clear any previous settings
P3OUT = 0; // Initialize port outputs to low state
P4REN = 0; // Pull-Up/Pull-down Resistors Disabled on P4 ports
P4SEL = 0; // Clear any previous settings
P4DIR = 0; // Clear any previous settings
P4OUT = 0; // Initialize port outputs to low state
ConfigureAdc(); // ADC set-up function call
__enable_interrupt(); // Enable interrupts.
while(1)
{
__delay_cycles(1000); // Wait for ADC Ref to settle
ADC10SA = (unsigned int)samples;
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
__bis_SR_register(CPUOFF + GIE); // Low Power Mode 0 with interrupts enabled
}
}
}
// ADC10 interrupt service routine
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR (void)
{
__bic_SR_register_on_exit(CPUOFF); // Return to active mode }
}
// Function containing ADC set-up
void ConfigureAdc(void)
{
ADC10CTL1 = INCH_4 + ADC10DIV_0 + CONSEQ_3 + SHS_0; // Channel 4, ADC10CLK/3
ADC10CTL0 &= ~(ENC);
ADC10CTL0 = SREF_0 + ADC10SHT_3 + MSC + ADC10ON + ADC10IE; // Vcc & Vss as reference, Sample and hold for 64 Clock cycles, ADC on, ADC interrupt enable
ADC10AE0 |= BIT4 + BIT3 + BIT2 + BIT1 + BIT0; // ADC input enable P2.4,P2.3,P2.2,P2.1,P2.0
ADC10DTC1 = 5;
}