Other Parts Discussed in Thread: MSP430F2132
Hi there
I'm using the MSP430F2132 in a current project and I've got a question regarding the sample and hold source for the ADC10.
In the User's Guide for the 2xx series, it says for the sample and hold source one of the following can be selected:
- ADC10SC
- Timer_A.OUT1
- Timer_A.OUT0
- Timer_A.OUT2
As there are 2 TimerA modules on the F2132, which one is the one that can be used as sample and hold source?
I suppose it's TimerA0, since TimerA1 only has two Capture/Compare Units and thus only two Output Units. But I can't find any information on that.
Regards
Roman