Other Parts Discussed in Thread: MSP430F2274
I need to get a minimum of 3.7V to the I/O pins to run sensors and an LCD screen and the maximum I am getting out of them now is 3.6. I was looking at the spec sheet and saw that the MSP430 has internal op amps which can adjust the gain to certain levels. My question is...does the op amp increase the voltage to the I/O pins so I can get the correct voltage to use the sensors or is it just an internal amplification?