Other Parts Discussed in Thread: MSP430FR4133, DAC7760
Hi all,
I am getting started on my Senior Design Project with my group. We are planning on building an ECG Simulator and then having the actual circuit to filter out the signal and output it onto an Android tablet for a "doctor" to take notes and draw stuff on the signal.
I will try to be very clear so that I can get as much advice as possible. I am working mainly on the simulator part in the beginning. I will be taking the open data from PhysioNet since they have several databases. I was planning on using about ten different records, up to a minute each. They have an option to print out the sample in text, which has anywhere between 150-350 samples per second. So for a minute, there will be about 21,000 lines of data for each sample.
The user would be able to use push buttons to scroll through the available sample signals, seeing the options on an LCD display, and then the microcontroller would output the signal, which would be dealt with after being output.
SO, I saw the MSP430FR4133 LaunchPad since it comes with two push buttons and a small LCD display. The struggle I am having is that I am wondering if you think I'll need a separate DAC to make the digital data into an analog signal to output to the electrode leads for the ECG. Also, is there enough memory on the microcontroller to store up to 10 of these sample signals?
If you have any input or advice at all, I will be very grateful. Let me know if you need to me to explain more clearly a part of the project.
Thank you very much.