This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 unique silicon ID - available in user code?



Is there a unique ID field anywhere in the MSP430 (F5529) that is available to the user? It would be very useful for unique product identification and security.

  • Yes, MSP430x5xx and MSP430x6xx have unique LotWafer / DieX / DieY combination inside TLV structrure (DIE record). There is device descriptors (TLV) table inside each device datasheet.

    Get Device
    # JTID Fuse Device Core Hard Soft LotWafer DieX DieY
    0  91   OK   3081  2106  10   10  B7A50951 0A00 1100
    1  91   OK   5435  0100  10   10  ADE98146 0A00 2100
    2  91   OK   3080  1104  30   10  B15B9446 2000 1700
    3  91   OK   3180  1104  12   12  013BB046 1200 1E00
    4  91   OK   5435  0100  10   10  ADE98146 0400 2000
    5  91   OK   3881  1106  10   10  219CA446 1800 0F00
    6  91   OK   3180  1104  12   12  013BB046 0D00 1E00
    7  91   OK   3180  1104  12   12  013BB046 2A00 2100

**Attention** This is a public forum