Other Parts Discussed in Thread: MSP430FR69891
We’re reading through the MSP430FR69891 spec and wasn’t clear on how to program the inputs for the device. It indicates that there are internal pull-ups for the input lines but doesn’t indicate whether or not we should be programming them with internal pull-ups if we have external pull-ups as well.
For example, if we have a GPIO line with an external pull-up resistor on it, do we program that input to be an “input with pull-up” or as a normal input? I was guessing that we program it as an input (without pull-ups) and let the external resistor do its job. However, it could be read that since it has an external pull-up, we have to program the pin to indicate that the input is an “input with pull-up.”