Other Parts Discussed in Thread: MSP430F5324, CC1101, CC1121
Hi,
I wish I could update a firmware of a device that is equipped with a micro(MSP430F5324), a wireless chip (CC1101 or CC1121), and an EEPROM-I2C 512Kbit.
The idea is to transmit the firmware to the device in wireless mode. the device will save the data in the EEPROM. At the end of the transmission the device will perform a consistency check of the firmware into the EEPROM (using a checksum for example) and if ok start the firmware update process taking data from the EEPROM.
Can you indicate me some documentations, application notes etc about this arguments.
Thanks.
Thomas