Other Parts Discussed in Thread: MSP430F5438
As I am fresher, I don't know how to interface SDI-12 with MSP430F5438 using GPIO. Please Suggest me... to make it possible...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5438
As I am fresher, I don't know how to interface SDI-12 with MSP430F5438 using GPIO. Please Suggest me... to make it possible...
Hi,
The SDI-12 interface uses a single bi directional serial data line that requires 0V and 5V levels. Generally the MSP430 GPIO lines are driven between zero and the processor Vcc, which is normally 3.3V or lower.
You will therefore need a hardware interface to get the basic voltage levels correct. A quick google search provides http://www.daycounter.com/Circuits/SDI-12/SDI-12-Interface.phtml which looks reasonable.
Once you have the required hardware you should be able to use the UART in the MSP to assist in generation the required serial bit stream for communications
Most of the new sensors from decagon run on 3 volt, so software driver is also a option now,
is it better to use software based interface or hardware based interface like daycounter circuit ?
**Attention** This is a public forum