Other Parts Discussed in Thread: MSP430G2231, MSP430F2370
Hello,
I am trying to load a program on to msp430f2370 using BSL pins but not had any success. I have the hardware setup exactly as in slaa535a.pdf. I am using the launch pad with msp430g2231 on it. After i flash the program on to the launchpad and then make connections with msp430f2370 hardware as shown in the document and power up, both green and red leds come on and remain that way as indicated int the document.
But, i am unable to get the bsldemo2 to work. when i run the command bsldemo2 -cCOMxx, i get 'synchronization error'.
My connections are correct. Checked them many times. Also ensured that the comport no. i am using is correct.
I do not know where i am going wrong. Is bsldemo2 supposed to work as is with msp430f2370? If not, can you please suggest an alternative method?
Thanks,
vinay