This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Nice to meet you.
We are developing the product with TI MSP430F6659 MCU.
We have some questions for the default TI USB BSL of MSP430F6659 MCU as follows:
1) Is the default TI USB BSL pre-programmed in the flash of MCUs before shipping to us?
2) Is the default TI USB BSL pre-programmed in the MCU same for every MCUs?
So, we can duplicate the default TI USB BSL in a MCU and program it into the other MCUs without modification.
Thank you.
Hank Chu said:1) Is the default TI USB BSL pre-programmed in the flash of MCUs before shipping to us?
Yes.
Hank Chu said:2) Is the default TI USB BSL pre-programmed in the MCU same for every MCUs?
If you mean "Do all MSP430F6659 devices have same BSL?" then yes. A BSL from a different device type probably won't work. While the source package is common, memory maps etc aren't. Therefore the source is compiled for each target device.
Hank Chu said:So, we can duplicate the default TI USB BSL in a MCU and program it into the other MCUs without modification.
Other than to replace a BSL that was accidentally erased, why would you need to?
**Attention** This is a public forum