I would like to get information about the EVM430-F6779 ZigBee communication specs.
We adquired a TI Meter (EVM430-F6779) and I need to use it with a group of third party ZigBee modules that are already installed. My question is: can I use the CC2530 module in order to communicate the EVM430-F6779 with the rest of the Third Party ZigBee modules? would there be issues regarding the TI Z-Stack protocol compatibility with others protocols?
If the answer is No: can I make an adaptor in order to conect a certain ZigBee module to the EVM430-F6779? what would I need and what would be the specs/steps needed to accomplish that?
Thanks in advance,
Best regards.