Other Parts Discussed in Thread: MSP430F2013, MSP-EXP430F5529LP
Hello. I want to use eZ-FET lite from LP to debug my own board with MSP430F2013. Previously I used MSP-FET430UIF and it works fine.
I made cable to connect from LP to JTAG header on my PCB. The schematic is:
LP JTAG on my PCB
GND----------9 GND
3.3V-----------2 VCCTOOL
SBW RST----1 TDO/TDI
SBW TST----7 TCK
I am not sure about connection of pin 8 TEST/VPP on JTAG header, so I left it unconnected.
Cable is 20 cm long.
The problem is that IAR EW MSP430 5.50.2 doesn't see eZ-FET lite. I check it in Project->Options->FET Debugger->Setup->Connection->...
There is only "Automatic" and not COM port of MSP Debug Interface. Although on wiki page of EZ-FET lite is said that it needs "IAR Embedded Workbench 5.50 or higher".
I tried to program my PCB with IAR EW MSP430 6.10.2. This version is not convenient for me now, but it sees eZ-FET lite and looks like it works good. I programmed and debugged my PCB with it.
How can I use IAR EW MSP430 5.50.2 with eZ-FET lite on MSP-EXP430F5529LP?