Hi,
I need to implement LPM mode. In which RTC,GPIO,UART should functional. I think LPM 3 can be implemented to meet the requirement.
1.Is LPM 3 meet my requirements?
2.Is it possible work UART at a baud rate of 115200 at this mode?
3.Is it possible to set 3 independent alarm for rtc in this mode?
I could see that in LPM mode 3 only ACLK is enabled. Using ACLK (32Khz) the maximum baud rate will be 9600. Can anybody suggest any alternative if any?
thanks in advance