This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F67791 SD24 input Buffer

Expert 2355 points

Hi,

Input impedance of SD24 is 400kohm in case of Diffential input in datasheet.

 

This 400kohm is Fig29-5

Figure 29-5. Analog Input Equivalent Circuit

http://www.ti.com/product/jp/MSP430F67791

1) Is 'F67791 implemented Buffer amp as below Fig.29-5?

2)Is Input impedance (=400kohm in the D/S)  equal to buffer amp input impedance?

best regards,

kyt

  • The comment in the posted schematics reads "see the device-specific data sheet". I suggest following this recommendation. Does the data sheet tell about buffered inputs or not? If not, then not. :)
    Hint: nothing in the datasheet indicates that there could be input buffers.
    This also makes question 2 void.

**Attention** This is a public forum