Has anyone managed to build the Energy Code library using IAR 6.10?
When i start rebuilding the 47197 toolkit there are 2 errors.
One for the greater version of the IAR compiler,
Fatal Error[Pe035]: #error directive: Compiler not recognised. C:\Users\Jorg\Desktop\slac488\Code Library\emeter\emeter-toolkit\include\isr_compat.h 85
which i suppose is resolved through modifying isrcompat.h?
And one
Error[25]: #error '"Must define USE_LARGE_CODE_MODEL (to either 0 or 1)."'. C:\Program Files\IAR Systems\Embedded Workbench 7.0\430\INC\macros.m43 23
How the last one can be resolved?