Hi,
i would like to use the MSP430 FR4133 launchpad together with the BOOSTXL-SENSHUB. I hope that both devices are compatible.
I suppose that the boosterpack sensors are only accessible through the I2C bus. Is this the only option?
Regards
Edgar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
i would like to use the MSP430 FR4133 launchpad together with the BOOSTXL-SENSHUB. I hope that both devices are compatible.
I suppose that the boosterpack sensors are only accessible through the I2C bus. Is this the only option?
Regards
Edgar
Hello again,
i am using the default jumper settings of the MSP430FR133 launchpad, i.e. power supply is from USB through the eZ-FET debugger.
Executing the program from the debugger GUI often produces the results described above. When the program is executed by unconnecting the launchpad after code download and reconnecting the board, accessing sensors of the BOOSTXL-SENSHUB through I2C works properly.
As such, debugging is very time-consuming.
Regards
Edgar
**Attention** This is a public forum