Hi everyone,
for my actual project I have to debug a MSP430FR5969 at a supply voltage of 2V. Therefore I bought an MSP-FET. Now the problem is that I can’t upload/debug the code. Most of the time I get the error “Unknown device”, even if I connect the MSP-FET to my MSP430FR5969 Launchpad. I’ve already read many post here which seems to deal with the same problem but I didn’t really find an answer. Do I have to change any settings in the CCS6 for example for 2 wire JTAG? Is there a problem with the security fuse?
Thanks in advance!
Simon