Other Parts Discussed in Thread: MSP430F1611, MSP-FET
Hi,
it may be a basic question but I am not sure I understood the difference between the green bug and the green triangle when you are willing to flash the program you wrote into the microcontroller. I wrote a code for SPI communication between MSP430F1611 and a Bluetooth low energy module. I then connected the jtag interface to the microcontroller pins in order to be able to flash (upload/burn) the program on it. If I click the green bug nothing happens but as soon as I click the green triangle almost right next to it (the one used to RUN the code) it immediately starts to run and it works perfectly. I am afraid that it should work only clicking the green bug, right? Which is the actual difference between the two?
Thanks.
Claudio.