Hi,
I was working on the launchpad and decided to power the chip without it and wrote a simple program on IAR.
All I do is stop the watchdog timer and turn on the LED1 port and then an infinite loop (tried asm and C). When I power the chip on launchpad either with usb or external power the LED1 port voltage is VCC. When I take the chip off and put it on the breadboard and power it up it's VCC/2. After checking on the oscilloscope I realized that it's (P1.0) alternating. Tried both on G2231 and G2211.
Thanks for the help guys.