This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am interested in implementing a CAN bus on an MSP430F2619-HT in a harsh environment, with 200C temperatures. I have found numerous CAN transceivers such as SN65HVD233-HT and SN65HVD1040-HT that fit the bill, but am having no luck finding a suitable CAN controller.
I know there are a few temperature rated MCUs/DSPs that have built in CAN, but they are nearly 10x as power hungry as the 430 I'm currently using, so I'd rather just add the CAN functionality through an SPI interface or similar instead of changing processors. I would probably be looking for something similar to the MCP2515. Is there such an animal?
Hi Brian,
Seeing this earlier post: MSP430 and CAN - MSP low-power microcontroller forum - MSP low-power microcontrollers - TI E2E support...
Other than this, I know there are other SPI to CAN interfaces on the market, you would just need to find one that will work with the logic levels of the MSP430 and is rated for the conditions you mentioned.
Best of luck,
Katie
**Attention** This is a public forum