How easy is it to load code onto the chip can i use the Launchpad dev kit? Im fairly new to all this so please be patient with me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dan:
You may want to consider using the MSP-EXP430G2 launchpad.
It can run twice as fast as the F1232, has twice the memory, both Flash and RAM.
Also, the launchpad is cheap compared to purchasing the tools necessary for the F1232.
There is also a good video course on getting started: http://processors.wiki.ti.com/index.php/Getting_Started_with_the_MSP430G2553_Value-Line_LaunchPad_Workshop
Hopefully, that helps.
Dan:
So, you have an existing board that contains an MSP430F1232IPW, correct?
Does that board have a JTAG connector, or place to solder on a JTAG connector?
(The 1x chips require a 4-wire JTAG for programming as I remember...)
Do you have an existing JTAG? (Should probably be MSP-FET430UIF or similar)
Dan:
Is there a specific reason for using the F1232? (Prior use?)
When you build your PCB, if you use the F1232, you should look at the TI board that will support it, and try to make some room on the board for a JTAG connection. That way, you can make changes to your code if you need to. For instance, the TI recommended evaluation board is MSP-FET430U28 - that board has a JTAG port, and the schematic can show you how to add the same to your PCB.
You could also consider comparing the Launchpad processor against the F1232 to see if there are enough similarities to move to the G2. (Besides the reasons I mentioned earlier, it is also half the price of the F1232.)
Dan:
Here is an FYI: http://dangerousprototypes.com/2012/12/19/sensorless-brushless-dc-motor-drive/
Not sure if this does much for you other than throwing in the confusion factor, but it did look interesting...
**Attention** This is a public forum