Other Parts Discussed in Thread: OPA376, MSP430F5438, MSP430FR5969, DIP-ADAPTER-EVM
Hey E2E,
I am working through the Simple DAC LaunchPad Project and would like to breadboard the following low pass filter cascade listed on the project page:
Can the OPA376 be prototyped on a solderless breadboard? If not, will someone please recommend a substitute IC Op Amp that can be prototyped on a solderless breadboard?
Once I get this project rolling, I intend to use it to design waveforms that can output to another MC(the MSP430FR5969 launchpad or the MSP430F5438 experimenter board) which has a VCC range of 1.8- 3.6 V.
I have converted this project code to use driverlib functionality. Are there any glaring drawbacks of using driverlib when initially learning to work with MCs?
Best regards,
Z