Hi,
I don't know how to describe the problem. I have 2x MSP430G2 v1.4 LaunchPads. One has MSP430G2231 and the other has MSP430G2211 running. I've written a simple programming polling TAIFG bit and toggling LEDs one on the left every second (G2211) the one on the right every half second (G2231). Capacitance is set to 12.5 pF. There are several problems. The crystals sometimes work and sometimes don't. If they do work, they sometimes stop. For some reason when I upload the program now and power up the LaunchPad via Flasher, the reset button doesn't work.
And the last one that makes me create a thread here is that when I connect both the LaunchPads to the same USB power adapter, and when the crystals are stuck if I touch the board's (with G2211) USB the other one starts working. The crystal stops resonating again after I take my finger off. If I put my finger on it again, it starts resonating from where it left resonating. Could it be my body's capacitance, my body being an antenna, the RF signals the university tower is emitting and the board is picking, GND issue with the USB power adapter or with universities system, or the combinations of all? This behavior is similar.
Some more notes: I've also tried 10 pF capacitance which seems to be fine for now on G2231 and not so fine on G2211.
P.S:The video was processing at the time I created this thread.
Murat