Other Parts Discussed in Thread: MSP430FR5722
Hello,
I am a student attempting to get an MSP430FR5722 attached to a custom PCB to connect to the MSP FET-Emulator tool. I have had no luck getting it to connect after multiple attempts. I have verified that the header I'm using to connect to the PCB is connected to the correct pins on the debug tool, that there are no shorts between the pins, and that there is continuity between the PCB header pins and the corresponding pads on the MSP430. We are using the IRGER package, so it is a little difficult for us to do resolder work.
Is there anything special I need to do in Code Composer Studio in order to get the FET to recognize the MSP? Are there any tests we can do to determine if the MSP's internal circuitry has been damaged? If the maximum reflow temperature is listed at 260c and it was heated to 265c, is it possible that something was broken internally? I'm at a loss as to why this isn't working.
I have attached my schematic for the connections to the MSP for reference.MSPcontrol.pdf
Thank you in advance for your help.
-Chris Hack