I am using a F5529 LaunchPad to read 3 EP4 optical encoders that require +5VDC, Will the input handle 5V or does it need to be reduced to 3.3 or 3.6?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using a F5529 LaunchPad to read 3 EP4 optical encoders that require +5VDC, Will the input handle 5V or does it need to be reduced to 3.3 or 3.6?
The msp have protection diodes and will channel away voltages over 3.6V (Vcc+0.3V)
But the diodes are limited to 2mA, so a 2K minimum series resistor is needed
I would use 100K (unless it's high-speed signal) as the excess voltage needs to be used up and as most LDO's (the one you use for MSP's Dvcc)
can not sink overvoltage's, so if the system is very energy efficient you could end up raising Dvcc to 5V and create permanent damage.
**Attention** This is a public forum