Other Parts Discussed in Thread: MSP430G2153
Hi
A short summary is: I need a specification for the protocol used to program MSP430 over a 5 pin interface (Spy-Bi-Wire).
The long version is: I want to develop a stand-alone PCB tester/programmer ("Test Box") that will, via a multitude of test pins, perform the following functions on production boards:
1. Test various parameters of the test specimen (internal voltage, current consumption etc);
2. Program in a "Test Program" to the MSP430G2153. This will not be the final program, but will allow the test specimen to exercise its hardware in a way which is not the final product operation but in a way which allows the Test Box to make various measurements easily.
3. One the "Test Program" is there, the Test Box will make suitable measurements and calculate appropriate values for some parameters.
4. The Test Box will then erase the Test Program.
5. The Test Box will then program in the Final software to the test specimen, which software will have been modified as required incorporating various results from the measurements performed at 3.
6. The Test Box will then perform one or two further tests.
7. The Test Box will then code protect the MSP430G2153.
The need for it to be standalone (no PC connected) and to have our own custom hardware for the various test.measurements, leads me to believe there is unlikely to be anything 'off the shelf' available for this, and we will have to design a special equipment to program the MSP430. We already do this for Atmel AVR chips on other products.
What I am having trouble finding is a specification for the protocol used to program the MSP430G2153. Does anyone know if it is available? The test specimens have 5 contacts available and thus far I have used MSP-FET430UIF for development programming/debugging with this 5 pin interface. I believe the interface is called "2-Wire JTAG Communication (Spy-Bi-Wire)". The pins used on the microcontroller are four in number: GND, VCC, Reset and Test/SBWTCK.
Thanks
Tony