Hi all,
please could someone explain me next behavior on msp430 (code bellow). I expected tha value in var_unit should be 0x3412, but it is 0x1200.
I know all msp430 are little endian and therefore this byte order, but I am pointing to byte with value 0x12 and second byte should be 0x34.
Please help me with this elentar issue. Thank in advce for replay. David
#include "stdint.h"
unsigned char buffer[6] = {0x00,0x12,0x34,0x56,0x78,0x90};
int main(void) {
volatile unsigned int var_uint = *((unsigned int *)&buffer[1]);
//value in var_int is 0x1200 return 0;
}