This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

when use printf("...\n") will suspend at "trgmsg.c" ?



Use CCS V6.0.1. By using FR5949, without using any setout breakpoints conditions. If I let “UCS” run 8Mhz ( CSCTL1 = DCOFSEL_6;) , the printf() won’t stop itself, but under “UCS” running under 16Mhz (FRCTL0 = FWPW | NACCESS_1; CSCTL1 = DCORSEL | DCOFSEL_4;) conditions, the printf()

will stop itself at line 90 (at trgmsg.c (i = 0; i < length; i++) PACKCHAR(*data++, p, i+8))

can you tell me why it causes that problem?

The test are as followed:

/*
* main.c
*/
#include <msp430.h> #include <stdio.h>
int i;
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer

PJSEL0 |= BIT4;
PJSEL0 |= BIT5;

FRCTL0 = FWPW | NACCESS_1; //---16MHz //8MHz not use

CSCTL0_H = CSKEY >> 8; // Unlock CS registers
// CSCTL1 = DCOFSEL_6; // Set DCO to 8MHz //---8MHz //16MHz not use
CSCTL1 = DCORSEL | DCOFSEL_4; // Set DCO to 16MHz //---16MHz //8MHz not use
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL4 &= ~(LFXTOFF + VLOOFF); // Enable LFXT1, VLO ON
do {
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1&OFIFG); // Test oscillator fault flag
CSCTL0_H = 0; // Lock CS registers

for (i=0; i<100; i++){
__delay_cycles(16000000);
printf("i=%x\n", i);
}
return 0;
}

  • What is NACCESS_1? It is the waitstate bit setting for 57xx family.
    FRCTL0 register has NWAITS bits. At least according to slau367f. pdf
    Since you don't get a compiler error, you might have included the wrong header file and compiled the code for an FR57xx device rather than the FR5949? If you somehow managed to mess this up, anything can happen if you execute the resulting code.

**Attention** This is a public forum