This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Getting started with Wireless Dev Tool EM430F6137RF900 with IAR kickstart

Other Parts Discussed in Thread: CC430F6137, MSP430F5419

Hello, I am new to using the MSP430.  

I just received my EM430F6137RF900 and MSP-FET430UIF USB Debug Interface.

I've downloaded IAR kickstart for MSP430 4.21.

I try to run the sample application that comes with IAR in the following location, by opening the workspace file

Program Files\IAR Systems\Embedded Workbench 5.4 Kickstart\430\FET_examples\FET_example\Flashing the LED.eww

Here's where I run into trouble.

if I select the MSP430x5xx (asm) - Debug workspace

I can compile just fine. But when I click on Project -> Download and Debug I get warning: Chosen derivative (MSP430F5419) and actual hardware (CC430F6137) do not match. Continue to download?

If I say Yes, it downloads and then I get a Stack Warning: The stack plug-in failed to set a breakpoint on "main".  The Stack window will not be able to display stack contents. (You can change this setting in the Tools>Options dialog box.) [OK]

Then Debug menu is available, I click on Debug->Go and the LED starts flashing as expected. 

I am not so worried about those warnings.  But the problem is that I would like to run project MSP430x5xx (C) or MSP430x5xx (C -SpyBiWire) since I will be writing my code in C and not assembly.

When I select the MSP430x5xx (C) project, again I can Rebuild All just fine, but when I click on Project->Download and Debug, I get the same warning. Chosen derivative (MSP430F5419) and actual hardware (CC430F6137) do not match. Continue to download?

If I say Yes, a small window that says "Downloading application..." appears and it just sits there.  I leave it alone for a few minutes, and nothing happens, then it says (Not responding) and IAR crashes. and I have to start over.

can anybody tell me what I have to do to get the c application to run? Also what is the difference between these two MSP430x5xx (C) or MSP430x5xx (C -SpyBiWire) ??

Thanks!

Emge

**Attention** This is a public forum