hi,
working on the code of glass break algorithm being provided by TI. right now the operation performed by the code is not stable.
i am trying to control the thud ,as so far thud is being continuously detected by the code.so i made some calibration and stopped the continuous detection so now the whenever the glass break sound is played only then thud is detected.
but this calibration values are not stable. i am just adding an offset to op-amps values for the calibration. so i calculated this calibration values at certain voltages. But after some time the calibration values changed to something different so anybody knows the reason behind it?