Other Parts Discussed in Thread: RCV420, TIDA-00247, TIDA-00165, TIDA-00095
Hi,
One of our customer's application needs to collect data from a Sensor to MCU.
The sensor's output options will be 4-20mA or 0V to 5V or -10V to +10V.
(Two Isolated sensor channels)
I was wondering if anyone implemented a receiver with MSP430's ADC
with a resolution of 1/4000 or 1/8000. There is a 4-20mA receiver IC(RCV420) from TI.
But we are looking for a all the possible solutions and if it is possible to build a Current Loop Receiver
with MSP's ADC and also with a switch option to change the input as 4-20mA or 0V to 5V.
Please let me know if there is any reference and suggestions to choose the necessary components.
Best Regards
Kummi.