This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linker error in attaching assembly file to C project

Hi all.
I have a known working c project.

It was requested of me to make an assembly module for the ADC we are using partially for our own learning, and partially because we use some micros programmed entirely in assembly.

I have created ADS1271asm.asm.  Currently I am just trying to test basic functionality and so i've created a function to return the absolute value of the passed variable.

in my main.c I have created the prototype:
extern Uint16 _abs_value_asmfunc(Uint16 value);
And have called the function:
ABS_VALUE = _abs_value_asmfunc(GARBAGE_DATA);

When I build main.c, and ADS1271asm.asm as individual files, both build properly.  When I build the project, I get the familiar error #10234-D: unresolved symbols remain, citing that:


 undefined           first referenced
  symbol                 in file     
 ---------           ----------------
 __abs_value_asmfunc ./main.obj  

Which usually means it's a linker error or definition error.  I'm pretty certain it's a linker error, as I have my function defined as above in main.c, and I'm stumped what I'm missing.

lastly, here is my assembly code in it's entirety, with commented out sections (tab formatting got a little wonky here):
;-----------------------------------------------------------------------;
;                                                                          ;
;                            DATA AREA                                      ;
;                                                                          ;
;-----------------------------------------------------------------------;
;section .data        ;Section for declaring initialized data or constants
;
;SETC OBJMODE        ; Set to C28x enhanced mode
;.retain
;.retainrefs
;-----------------------------------------------------------------------;
;                                                                          ;
;                            BSS AREA                                      ;
;                                                                          ;
;-----------------------------------------------------------------------;
;section .bss        ;Section for declaring variables
    .def    _abs_value_asmfunc
;    .sect    "ramfuncs"
    .global _abs_value
    .global __abs_value_asmfunc
;
;
;-----------------------------------------------------------------------;
;                                                                          ;
;                            CODE AREA                                      ;
;                                                                          ;
;-----------------------------------------------------------------------;
;section .text        ;Section used for keeping functional code

_abs_value_asmfunc:

    CLRC    TC                        ;Clear TC flag, use as sign flag
    MOV        ACC, @_abs_value << 16    ;Shift variable up to AH
    ABSTC    ACC                        ;Take absolute value
    NEGTC    ACC                        ;Negate ACC if TC=1

    LRET                            ;Return from address on stack



Couple final questions:
when I take out the comments for section .bss (but not .data) I get the error:
"../ADS1271asm.asm", ERROR!   at line 42: [E0005] Operand missing

If I take out the comments for section .text, I get the error:
"../ADS1271asm.asm", ERROR!   at line 54: [E0300] Symbol section has already been defined

commenting out both .bss and .data will allow the file to compile.

Lastly, I have read through the following TI documents:
CPU Instruction set
Optimizing C Compiler
C28x Assembly Language
Easy Way of Creating a C-callable Assembly Function

Any help you can offer would be appreciated.

-Cam Buskell



  • Cam Buskell said:
    ;SETC OBJMODE        ; Set to C28x enhanced mode
    ;.retain

    ..................................... SNIP .........................

    ;                            CODE AREA                                      ;
    ;                                                                          ;
    ;-----------------------------------------------------------------------;
    ;section .text        ;Section used for keeping functional code

    _abs_value_asmfunc:

        CLRC    TC                        ;Clear TC flag, use as sign flag
        MOV        ACC, @_abs_value << 16    ;Shift variable up to AH
        ABSTC    ACC                        ;Take absolute value
        NEGTC    ACC                        ;Negate ACC if TC=1

        LRET                            ;Return from address on stack

     Hi CAM, are you sure this is MSP430? It seems a c2000 code and also the c28x directive and document you mentioned are relative to C2000, I fear you posted on wrong forum.

     I never used C2xx asm and also I am forgetting MSP too in favour of C.

  • ... nope. I posted in the wrong forums, my apologies.

    should be in the c2000.
  • Though I did find the issue.
    variables and functions declared in C should not have the underscore prefix.
  • Cam Buskell said:
    variables and functions declared in C should not have the underscore prefix.

     Happy to see you solved issue of naming.

**Attention** This is a public forum