Other Parts Discussed in Thread: MSP430FR5969
Could anyone tell me the interrupt number for TA1CCR0 CCIFG0 word address 0FFEAh?
Below is the datasheet for the MSP430FR59XX:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430FR5969
Could anyone tell me the interrupt number for TA1CCR0 CCIFG0 word address 0FFEAh?
Below is the datasheet for the MSP430FR59XX:
Rodney Wong said:Could anyone tell me the interrupt number for TA1CCR0 CCIFG0 word address 0FFEAh?
What do you mean whit this phrase?
If it is the table position then you can get from address, (0xfffe-Address_Of_Vector)/2
If it is the vector value then this is the address of service routine and must be set from compiler directive..
Hi Roberto,
I am trying to fill this form from the sys/bios app.cfg:
The workshop manual that I am using says that the interrupt number is suppose to be under the priority. However, there is no number. Only Highest and lowest is under priority. Do you suppose the I could set the number manually? And how would I do that?
Look into the <msp430fr5969.h> header file:
#define TIMER0_A0_VECTOR (46) /* 0xFFEA Timer0_A3 CC0 */
Rodney Wong said:I see. However, my 0xFFEA was defined for timer a1 and as 41.
Right, so I grasped what you intended with interrupt number. Effectively some form of automate can be useful, but considering that task is set one time per project can be acceptable. (after one has learned where to seek information for every processor family is using.)
**Attention** This is a public forum