Hi !!
I have working with EVM 6779 code which currently samples and measure v & i sample with a OSR = 256 i.e 4096 samples per sec and each sample at 4.394 degree.
I wanted to sample at around 5 degree with OSR = 291 or at 3 degree with OSR = 175. I have modified the samples_per_second value accordingly as 3603 or 5992. But I am unable to get the result which i had with OSR=256.I am getting a lesser value with OSR = 291 or 175 .
Can anyone tell ..where have i gone wrong or what else do i need to modify in the code...say for 3 degree.
Thanks & Regards,
Ars..