This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Everyone
I am working on a feature that utilizes Bluetooth to do the firmware upgrade. This could be very exciting since it's the most easiest way for customers to update the program. Our ideal scenario is that customers click one button on the app then the system updates itself. The customer will not need push any button or looking into the tedious user manual...
Since we are using a 'transparent' bluetooth module (which means whatever I send from App, it will send to MCU through UART), the upgrade process can be controlled through the App. Except, however, it requires start sequence to initialize the upgrade process.
I am wondering is there anyway to generate the start sequence? We do have another MCU (a separate MCU for other purpose). It'll be possible to generate the start sequence from that MCU, but this solution let me feel not fail-safe....
Welcome any suggestions!
Kevin
**Attention** This is a public forum