Other Parts Discussed in Thread: MSP430F5438A, MSP430F5418A
Hi all,
We've got an MSP430F5438A chip on our own board with JTAG and CANBUS communication (read: no UART comms).
I'm attempting to write a BSL that allows for program upgrades via CANBUS but I seem to have something fundamentally incorrect.
I've based my code on example shown in the custom BSL wiki (processors.wiki.ti.com/index.php/Custom_MSP430_BSL), but it appears to me like the BSL protect function does not get run.
In an effort to determine if the BSL protect function is run, I've modified it to simply erase the info b segment.
The assembly code I use to clear info b is known to work as I can call it from C++, and it clears the "RUNBSL" string from flash.
My process is: memcpy "RUNBSL" to 0x1900 (6 bytes), memcpy 0xC35A to 0x17F6 (2 bytes), memcpy 0x3CA5 to 0x17F4 (2 bytes), and then manually power cycle the device.
I know the values are written correctly as I have my code read those locations and send CANBUS messages to my PC with the values.
I also see the values there through the CCS debugger.
It simply appears that the BSL Protect function is not run as the "RUNBSL" string is still there when the main application runs again.
Another oddity (I'm not sure this is related but felt it was worth mentioning) is that the .asm file specifies the C35A/3CA5 values for the locations 0x17F4/0x17F6, but those values are not there when the software is flashed and runs.
I have to write those values with the same function that writes the "RUNBSL" string to 0x1900.
Any ideas what I'm doing wrong here?
Attached is the relevant code (mem_map.cmd renamed to mem_map_cmd.txt so it would upload).1715.sb_assembly.asm1715.app_code.cpp
/* ============================================================================ */
/* Copyright (c) 2014, Texas Instruments Incorporated */
/* All rights reserved. */
/* */
/* Redistribution and use in source and binary forms, with or without */
/* modification, are permitted provided that the following conditions */
/* are met: */
/* */
/* * Redistributions of source code must retain the above copyright */
/* notice, this list of conditions and the following disclaimer. */
/* */
/* * Redistributions in binary form must reproduce the above copyright */
/* notice, this list of conditions and the following disclaimer in the */
/* documentation and/or other materials provided with the distribution. */
/* */
/* * Neither the name of Texas Instruments Incorporated nor the names of */
/* its contributors may be used to endorse or promote products derived */
/* from this software without specific prior written permission. */
/* */
/* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" */
/* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, */
/* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR */
/* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR */
/* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, */
/* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, */
/* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; */
/* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, */
/* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR */
/* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, */
/* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */
/* ============================================================================ */
/******************************************************************************/
/* lnk_msp430f5438a.cmd - LINKER COMMAND FILE FOR LINKING MSP430F5438A PROGRAMS */
/* */
/* Usage: lnk430 <obj files...> -o <out file> -m <map file> lnk.cmd */
/* cl430 <src files...> -z -o <out file> -m <map file> lnk.cmd */
/* */
/*----------------------------------------------------------------------------*/
/* These linker options are for command line linking only. For IDE linking, */
/* you should set your linker options in Project Properties */
/* -c LINK USING C CONVENTIONS */
/* -stack 0x0100 SOFTWARE STACK SIZE */
/* -heap 0x0100 HEAP AREA SIZE */
/* */
/*----------------------------------------------------------------------------*/
/* Version: 1.127 */
/*----------------------------------------------------------------------------*/
/****************************************************************************/
/* SPECIFY THE SYSTEM MEMORY MAP */
/****************************************************************************/
MEMORY
{
SFR : origin = 0x0000, length = 0x0010
PERIPHERALS_8BIT : origin = 0x0010, length = 0x00F0
PERIPHERALS_16BIT : origin = 0x0100, length = 0x0100
ZAREA_MEM : origin = 0x1000, length = 0x0010
ZAREA_CODE_MEM : origin = 0x1014, length = 0x0050
BSLSIG : origin = 0x17F0, length = 0x0010
RAM : origin = 0x1C00, length = 0x4000
INFOA : origin = 0x1980, length = 0x0080
INFOB : origin = 0x1900, length = 0x0080
INFOC : origin = 0x1880, length = 0x0080
INFOD : origin = 0x1800, length = 0x0080
FLASH : origin = 0x5C00, length = 0xA380
FLASH2 : origin = 0x10000,length = 0x35C00
INT00 : origin = 0xFF80, length = 0x0002
INT01 : origin = 0xFF82, length = 0x0002
INT02 : origin = 0xFF84, length = 0x0002
INT03 : origin = 0xFF86, length = 0x0002
INT04 : origin = 0xFF88, length = 0x0002
INT05 : origin = 0xFF8A, length = 0x0002
INT06 : origin = 0xFF8C, length = 0x0002
INT07 : origin = 0xFF8E, length = 0x0002
INT08 : origin = 0xFF90, length = 0x0002
INT09 : origin = 0xFF92, length = 0x0002
INT10 : origin = 0xFF94, length = 0x0002
INT11 : origin = 0xFF96, length = 0x0002
INT12 : origin = 0xFF98, length = 0x0002
INT13 : origin = 0xFF9A, length = 0x0002
INT14 : origin = 0xFF9C, length = 0x0002
INT15 : origin = 0xFF9E, length = 0x0002
INT16 : origin = 0xFFA0, length = 0x0002
INT17 : origin = 0xFFA2, length = 0x0002
INT18 : origin = 0xFFA4, length = 0x0002
INT19 : origin = 0xFFA6, length = 0x0002
INT20 : origin = 0xFFA8, length = 0x0002
INT21 : origin = 0xFFAA, length = 0x0002
INT22 : origin = 0xFFAC, length = 0x0002
INT23 : origin = 0xFFAE, length = 0x0002
INT24 : origin = 0xFFB0, length = 0x0002
INT25 : origin = 0xFFB2, length = 0x0002
INT26 : origin = 0xFFB4, length = 0x0002
INT27 : origin = 0xFFB6, length = 0x0002
INT28 : origin = 0xFFB8, length = 0x0002
INT29 : origin = 0xFFBA, length = 0x0002
INT30 : origin = 0xFFBC, length = 0x0002
INT31 : origin = 0xFFBE, length = 0x0002
INT32 : origin = 0xFFC0, length = 0x0002
INT33 : origin = 0xFFC2, length = 0x0002
INT34 : origin = 0xFFC4, length = 0x0002
INT35 : origin = 0xFFC6, length = 0x0002
INT36 : origin = 0xFFC8, length = 0x0002
INT37 : origin = 0xFFCA, length = 0x0002
INT38 : origin = 0xFFCC, length = 0x0002
INT39 : origin = 0xFFCE, length = 0x0002
INT40 : origin = 0xFFD0, length = 0x0002
INT41 : origin = 0xFFD2, length = 0x0002
INT42 : origin = 0xFFD4, length = 0x0002
INT43 : origin = 0xFFD6, length = 0x0002
INT44 : origin = 0xFFD8, length = 0x0002
INT45 : origin = 0xFFDA, length = 0x0002
INT46 : origin = 0xFFDC, length = 0x0002
INT47 : origin = 0xFFDE, length = 0x0002
INT48 : origin = 0xFFE0, length = 0x0002
INT49 : origin = 0xFFE2, length = 0x0002
INT50 : origin = 0xFFE4, length = 0x0002
INT51 : origin = 0xFFE6, length = 0x0002
INT52 : origin = 0xFFE8, length = 0x0002
INT53 : origin = 0xFFEA, length = 0x0002
INT54 : origin = 0xFFEC, length = 0x0002
INT55 : origin = 0xFFEE, length = 0x0002
INT56 : origin = 0xFFF0, length = 0x0002
INT57 : origin = 0xFFF2, length = 0x0002
INT58 : origin = 0xFFF4, length = 0x0002
INT59 : origin = 0xFFF6, length = 0x0002
INT60 : origin = 0xFFF8, length = 0x0002
INT61 : origin = 0xFFFA, length = 0x0002
INT62 : origin = 0xFFFC, length = 0x0002
RESET : origin = 0xFFFE, length = 0x0002
}
/****************************************************************************/
/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY */
/****************************************************************************/
SECTIONS
{
.bss : {} > RAM /* GLOBAL & STATIC VARS */
.data : {} > RAM /* GLOBAL & STATIC VARS */
.sysmem : {} > RAM /* DYNAMIC MEMORY ALLOCATION AREA */
.stack : {} > RAM (HIGH) /* SOFTWARE SYSTEM STACK */
.text : {}>> FLASH | FLASH2 /* CODE */
.text:_isr : {} > FLASH /* ISR CODE SPACE */
.cinit : {} > FLASH | FLASH2 /* INITIALIZATION TABLES */
.const : {} > FLASH | FLASH2 /* CONSTANT DATA */
.cio : {} > RAM /* C I/O BUFFER */
.pinit : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.init_array : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.mspabi.exidx : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.mspabi.extab : {} > FLASH /* C++ CONSTRUCTOR TABLES */
.infoA : {} > INFOA /* MSP430 INFO FLASH MEMORY SEGMENTS */
.infoB : {} > INFOB
.infoC : {} > INFOC
.infoD : {} > INFOD
BSLSIG : {} > BSLSIG /* assembly code */
ZAREA : {} > ZAREA_MEM
ZAREA_CODE : {} > ZAREA_CODE_MEM
/* MSP430 INTERRUPT VECTORS */
.int00 : {} > INT00
.int01 : {} > INT01
.int02 : {} > INT02
.int03 : {} > INT03
.int04 : {} > INT04
.int05 : {} > INT05
.int06 : {} > INT06
.int07 : {} > INT07
.int08 : {} > INT08
.int09 : {} > INT09
.int10 : {} > INT10
.int11 : {} > INT11
.int12 : {} > INT12
.int13 : {} > INT13
.int14 : {} > INT14
.int15 : {} > INT15
.int16 : {} > INT16
.int17 : {} > INT17
.int18 : {} > INT18
.int19 : {} > INT19
.int20 : {} > INT20
.int21 : {} > INT21
.int22 : {} > INT22
.int23 : {} > INT23
.int24 : {} > INT24
.int25 : {} > INT25
.int26 : {} > INT26
.int27 : {} > INT27
.int28 : {} > INT28
.int29 : {} > INT29
.int30 : {} > INT30
.int31 : {} > INT31
.int32 : {} > INT32
.int33 : {} > INT33
.int34 : {} > INT34
.int35 : {} > INT35
.int36 : {} > INT36
.int37 : {} > INT37
.int38 : {} > INT38
.int39 : {} > INT39
.int40 : {} > INT40
RTC : { * ( .int41 ) } > INT41 type = VECT_INIT
PORT2 : { * ( .int42 ) } > INT42 type = VECT_INIT
USCI_B3 : { * ( .int43 ) } > INT43 type = VECT_INIT
USCI_A3 : { * ( .int44 ) } > INT44 type = VECT_INIT
USCI_B1 : { * ( .int45 ) } > INT45 type = VECT_INIT
USCI_A1 : { * ( .int46 ) } > INT46 type = VECT_INIT
PORT1 : { * ( .int47 ) } > INT47 type = VECT_INIT
TIMER1_A1 : { * ( .int48 ) } > INT48 type = VECT_INIT
TIMER1_A0 : { * ( .int49 ) } > INT49 type = VECT_INIT
DMA : { * ( .int50 ) } > INT50 type = VECT_INIT
USCI_B2 : { * ( .int51 ) } > INT51 type = VECT_INIT
USCI_A2 : { * ( .int52 ) } > INT52 type = VECT_INIT
TIMER0_A1 : { * ( .int53 ) } > INT53 type = VECT_INIT
TIMER0_A0 : { * ( .int54 ) } > INT54 type = VECT_INIT
ADC12 : { * ( .int55 ) } > INT55 type = VECT_INIT
USCI_B0 : { * ( .int56 ) } > INT56 type = VECT_INIT
USCI_A0 : { * ( .int57 ) } > INT57 type = VECT_INIT
WDT : { * ( .int58 ) } > INT58 type = VECT_INIT
TIMER0_B1 : { * ( .int59 ) } > INT59 type = VECT_INIT
TIMER0_B0 : { * ( .int60 ) } > INT60 type = VECT_INIT
UNMI : { * ( .int61 ) } > INT61 type = VECT_INIT
SYSNMI : { * ( .int62 ) } > INT62 type = VECT_INIT
.reset : {} > RESET /* MSP430 RESET VECTOR */
}
/****************************************************************************/
/* INCLUDE PERIPHERALS MEMORY MAP */
/****************************************************************************/
-l msp430f5438a.cmd