Other Parts Discussed in Thread: MSP430F5310, MSP-TS430PN80A
I am new to MSP 430. My application using MSP430F5310 at 3.6Vdc running at 8MHz and toggling between LPM3 and active mode. The firmware runs OK from debugger (Elprotronics+IAR5.60), but runs erratically when running stand alone with no debugger. \
-When i enabled PMM initialization using the firmware libraryfunction PMM_setVCore(1) - code runs with JTAg debugger but run erraticly without debugger.
-When i disable PMM initialization using the firmware library function PMM_setVCore(1) - code runs the same with or without debugger. But it is not useful to me as it prevents detection of reset source in SYSRSTIV - i get SVSL reset indication for some reason and thus can not detect if Watcdog reset occurred.
Any advice someone ?