This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help uart programming msp430fr5969



hello,

I am a new user of microcontroller msp430fr5969 and I need help in programming the uart. and i want to connect the msp430 with a bluetooth (PAN1026).
when I use a terminal to see what I get , I find þþþþþþþþþþþþþþþþþþ.
here is my code
#include "driverlib.h"

unsigned char TCU_HCI_RESET_REQ[4] = {0x01, 0x03, 0x0c, 0x00};
unsigned char i;
int main(void)
{

	WDTCTL = WDTPW | WDTHOLD;                 // Stop Watchdog

  P2SEL1 |= BIT5 | BIT6;                    // Configure UART pins
  P2SEL0 &= ~(BIT5 | BIT6);


  // Disable the GPIO power-on default high-impedance mode to activate
  // previously configured port settings
  PM5CTL0 &= ~LOCKLPM5;

  // Configure USCI_A0 for UART mode
  UCA1CTL1 |= UCSWRST;
  UCA1CTL1 = UCSSEL__ACLK;                  // Set ACLK = 32768 as UCBRCLK
  UCA1BR0 = 3;                              // 9600 baud
  UCA1MCTLW |= 0x5300;                      // 32768/9600 - INT(32768/9600)=0.41
                                            // UCBRSx value = 0x53 (See UG)
  UCA1BR1 = 0;
  UCA1CTL1 &= ~UCSWRST;                     // release from reset
  UCA1IE |= UCRXIE;                        // Enable USCI_A1 RX interrupt


  USART1_SendData(TCU_HCI_RESET_REQ,4);
  

}
void USART1_SendByte (unsigned char data) {
	while(!(UCA1IFG & UCTXIFG));

	UCA1TXBUF = data;
}
void USART1_SendData (unsigned char data[], unsigned char length) {
	unsigned char i;

	for(i=0; i<length; i++) {
		USART1_SendByte(data[i]);
		
	}
}

**Attention** This is a public forum