Hello. I work with MSP430 eZ430-RF2500-SEH. I downloaded the code on the access point and on end device. Thereafter, the end device is not connected to an access point. On the access point is flashing green LED on the end device both LEDs flash simultaneously. The program eZ430-RF2500 SEH sensor monitor shows that the bubble is not flashing, and nothing is displayed. How can I fix it?